This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP451-Q1: 工作原理咨询

Part Number: TMP451-Q1
Other Parts Discussed in Thread: TMP451

你好,请问tmp451的工作原理是什么样的?是tmp451输出电流,电流多大? 流经proceesor的bjt , 看 tmp451的pin2/3 的差分电压嘛? 电压跟温度(或者说寄存器的值)有什么关联呢。譬如1V对应的寄存器值是多少呢?

我们遇到一个问题,就是processor 还没有完全上电,tmp451 的 remote 就过温了,然后把therm pin 拉低,从而把processor的上电进程中止了, 读tmp451的寄存器,remote 温度的值为0x7f。 其他配置均为tmp451的默认值。因此超过了therm的limit值0x6e, 请问有什么原因会导致这种情况呢? 

我们测到的pin2/3的波形如下:

请问下图1中,约60ms周期的脉冲是什么原因造成的?

下图2,单个脉冲中高低电平有什么含义?

x 出现错误。请重试或与管理员联系。