This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944: HWA的干扰模块设置问题

Part Number: AWR2944


TI工程师您好,有些HWA使用干扰模块配置问题想请教下

1.通过写死sw-intf_loc_thresh_mag <n> _sw,INTF_LOC_THRESH_MAGDIFF<n> _sw,软件可以正常跑通,对于受到干扰的数值也被置0了;但阈值选择-INTF_LOC_THRESH_MAG<n>,INTF_LOC_THRESH_MAGDIFF<n>却无法把干扰置于0,这个n一共有12个,debug看寄存器内部n也只有前4个有数值,后8个都是0值,请问这个内部12个阈值是如何计算的?有详细说明吗?一个chirp信号所有的采样点进去算个abs(x)或者abs( xi − xi − 1) ,是每12个点累加一次?

2.INTF_MITG_RIGHT_HYST_ORD、INTF_MITG_LEFT_HYST_ORD这个是和CFAR的窗类似吗,例如INTF_MITG_RIGHT_HYST_ORD=2;INTF_MITG_LEFT_HYST_ORD=2,INTF_MITG_CNTTHRESH=1,是代表当前点、左边2个点及右边2个点,若5个点中的IIB个数超过1个,则认为受到干扰,不知道是不是这样理解的?

3.关于缩放问题,INTF_STATS_MAG_SCALE和INTF_STATS_MAG_SCALE是通过这个函数rangeProcHWADDMA_findIntfStatsStaticParams计算的,但看手册里INTF_STATS_MAG_SCALE默认设置是8,可函数中demo输出的是254,只有SNRdb是可调参数,这边254和8数值相差很大的原因是?且通过函数计算的最小值也不能到8这个数值?如果设置8,内部计算的阈值都偏小,另INTF_STATS_MAG_SCALE和INTF_STATS_MAG_SCALE有啥推荐参数吗