This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: 与DCA1000EVM连接,使用mmwave_studio_02.01.01.00,Trigger Frame的时候报错

Part Number: IWR6843ISK
Other Parts Discussed in Thread: DCA1000EVM

与DCA1000EVM连接,使用mmwave_studio_02.01.01.00,Trigger Frame的时候,出现以下报错:
[17:17:10] [RadarAPI]: ar1.StartFrame()
[17:17:10] [RadarAPI]: Status: Passed
[17:17:10] Frame start async event received!
[17:17:10] [RadarAPI]: Frame Ended
[17:17:39] [RadarAPI]:
[17:17:39] Frame End async event received!
[17:17:39] [RadarAPI]:
[17:17:39] Start Record command : Success
[17:17:39]
[17:17:39] No LVDS data
[17:17:39]
[17:17:39] Record stop is done successfully
[17:17:48] [RadarAPI]: ar1.StartMatlabPostProc("C:\\TI\\mmwave_studio_02_01_01_00\\mmWaveStudio\\PostProc\\adc_data.bin")
[17:17:48] [RadarAPI]: No of files Captured: 1, Total no of frames for each device : 8
[17:17:48] [RadarAPI]: Error:
[17:17:48]
[17:17:48] ... MWMCR::EvaluateFunction error ...
[17:17:48] Reference to non-existent field 'ChannelConfig'.
[17:17:48] Error in => process_adc_data.m at line 76.
[17:17:48]
[17:17:48] ... Matlab M-code Stack Trace ...
[17:17:48] at
[17:17:48] file C:\Users\GACU\AppData\Local\Temp\GACU\mcrCache8.5.1\Matlab0\Processing_functions\prepare_frame.m, name compute_size_per_burst_size, line 63.
[17:17:48] at
[17:17:48] file C:\Users\GACU\AppData\Local\Temp\GACU\mcrCache8.5.1\Matlab0\Processing_functions\prepare_frame.m, name compute_frame_sizes, line 45.
[17:17:48] at
[17:17:48] file C:\Users\GACU\AppData\Local\Temp\GACU\mcrCache8.5.1\Matlab0\Processing_functions\prepare_frame.m, name prepare_frame, line 19.
[17:17:48] at
[17:17:48] file C:\Users\GACU\AppData\Local\Temp\GACU\mcrCache8.5.1\Matlab0\Processing_functions\create_current_burst_config.m, name create_current_burst_config, line 5.
[17:17:48] at
[17:17:48] file C:\Users\GACU\AppData\Local\Temp\GACU\mcrCache8.5.1\Matlab0\Processing_functions\populate_current_burst_constants.m, name populate_current_burst_constants, line 11.
[17:17:48] at
[17:17:48] file C:\Users\GACU\AppData\Local\Temp\GACU\mcrCache8.5.1\Matlab0\MatlabPostPr\process_adc_data.m, name process_adc_data, line 76.
[17:17:48]
[17:17:48]
[17:17:48] Trace:
[17:17:48] 在 MathWorks.MATLAB.NET.Utility.MWMCR.EvaluateFunction(String functionName, Int32 numArgsOut, Int32 numArgsIn, MWArray[] argsIn)
[17:17:48] 在 MathWorks.MATLAB.NET.Utility.MWMCR.EvaluateFunction(Int32 numArgsOut, String functionName, MWArray[] argsIn)
[17:17:48] 在 MatlabPostProcGui.MatlabPostProcGUIClass.process_adc_data(MWArray adc_file_name, MWArray force_cont_stream_mode)
[17:17:48] 在 AR1xController.frmAR1Main.iStartMtlabPostProc()

C:\TI\mmwave_studio_02_01_01_00\mmWaveStudio\PostProc文件夹中adc_data.bin文件没有更新(之前成功收到数据过),但adc_data_Raw_LogFile.csv文件有新数据