This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWRL1432BOOST: 请问GPADC sampling time是什么含义

Part Number: AWRL1432BOOST


SWRS296A 文档中给出了GPADC的 sampling time为 300ns

假设 XTAL clock的时钟为40MHz,那么 采集一个sample的周期是1.203us, 那么ADC sampling time = 300ns是指哪部分时间?

ADC sampling time= 300ns,是否包含在  collect sample period之中?

  • 感谢您对TI产品的关注!
    关于你的咨询, 请参考下面的解释说明。

    The ADC sampling time is determined by two parameters in the chirpComnCfg: DigOutputSampRate and NumOfAdcSamples.
    This can be calculated by taking the number of ADC samples and dividing by the sampling rate.
    Note: the DigOutputSampRate specifies the decimator to be used to determine the sampling rate (sampling rate = 100 MHz/DigOutputSampRate).
    For example, if DigOutputSampRate = 32 (Sampling Rate = 3.125 MHz) and NumOfAdcSamples = 128, then the sampling time is 40.96 ns (128/3.125 MHz).

  • 感觉像是GPADC内部的 SARADC sampling 模拟信号的时间~