This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843BOOST: 使用mmWaveSensingEstimator进行参数估计时有问题

Part Number: IWR1843BOOST
Other Parts Discussed in Thread: DCA1000EVM, , IWR1843, IWR6843

使用mmWaveSensingEstimator进行参数计算中,我将最大检测距离设置为11.5m,距离分辨率为5cm,最大检测速度为26km/h,速度分辨率为0.2065km/h,根据其计算的结果,我使用iwr1843boost+DCA1000EVM配合mmwavestudio采集人体行走数据,但是测量完成之后,看mmwavestudio生成的fft图像以及点云图像发现最大检测距离只有6m左右,使用我自己的代码进行处理时也是只有6m左右。这是什么问题,怎么解决呢