This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243BOOST: 固件烧入

Expert 1655 points
Part Number: AWR2243BOOST
Other Parts Discussed in Thread: AWR2243

我通过FPGA控制AWR2243BOOST,可以用FPGA通过SPI烧入固件给AWR2243BOOST?固件怎么通过SPI烧入?

  • 感谢您对TI产品的关注!
    关于你的咨询,通过FPGA控制AWR2243BOOST,可以使用FPGA通过SPI烧入固件给AWR2243BOOST。

    确保你拥有适用于AWR2243BOOST的固件文件,通常这些文件是.bin或.hex格式。
    设置好FPGA的开发环境,包括必要的IP核、开发板和相应的开发工具链。
    在FPGA中配置SPI接口,确保它与AWR2243BOOST的SPI接口兼容。
    包括设置正确的时钟频率、数据位长度、CPOL和CPHA等参数。

    在烧录固件之前,通常需要通过复位脚控制AWR2243BOOST复位,以确保它处于可接收固件的状态。
    使用FPGA通过SPI接口发送固件数据到AWR2243BOOST。
    在发送过程中,需要遵循AWR2243BOOST的SPI通信协议,包括发送正确的命令、地址和数据。
    固件加载完成后,可以通过发送特定的命令或检查AWR2243BOOST的状态寄存器来验证固件是否已成功加载。


    注意下面的事项:
    确保使用的固件文件与AWR2243BOOST的硬件版本和配置兼容。
    SPI通信参数:在配置SPI接口时,务必确保所有参数都与AWR2243BOOST的要求相匹配。
    确保AWR2243BOOST和FPGA的电源和接地稳定可靠,供电充足,以避免因电源波动或接地不良导致的通信问题。

  • 固件是存在AWR2243BOOST哪一个部分,是在AWR2243芯片里面吗