This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243BOOST: AWR2243BOOST的XDS110这款芯片在与MMW studio连接时的作用

Part Number: AWR2243BOOST
Other Parts Discussed in Thread: AWR2243

工程师,你好:

    我利用AWR2243这款芯片,参照AWR2243Boost评估板做了开发,但是在我们使用自己开发的板子在连接MMW Studio软件进行雷达评估时出现了问题:

我们开发的板子能按照使用流程1.连接RS232;2.下载BSS、MSS固件;3.连接SPI。但是在后续的Power up时出现软件卡死的现象,控制台也没有任何报错或警告。

硬件上我们的板卡与评估板的区别为:

1.AWR2243Boost 的RS232通过XDS110转换为USB与PC MMW studio 连接;我们的板子是RS232通过单独的FT232RNL转接板连接至PC MMW Studio.

2.AWR2243Boost 的SPI通过DCA1000采集板的FT4232芯片转换为USB连接至PC;我们班的板子是SPI通过外部 单独的FT4232H转接板连接至PC MMW studio.

我的问题是:

1.我们出现power up异常的情况是否与XDS110有关?XDS110这款芯片的内部是否存有相应的与MMW studio 的应答协议?比如在MMWstudio点击Power Up或配置其他参数时需要XDS110相应的应答信号。

请问是否有相关描述XDS110功能的资料,如果有XDS110相应的固件,请问能否提供改固件。

2.SPI 与 HOST _INT信号是否有相应的控制应答协议?