This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243BOOST: module 'RSTD' not found

Part Number: AWR2243BOOST


OUTCOME
Failed to load RSTD module: ...1_01_00\mmWaveStudio\Scripts\DataCaptureDemo_xWR.lua:3: module 'RSTD' not found:
no field package.preload['RSTD']
no file '.\RSTD.lua'
no file 'C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\RunTime\lua\RSTD.lua'
no file 'C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\RunTime\lua\RSTD\init.lua'
no file 'C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\RunTime\RSTD.lua'
no file 'C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\RunTime\RSTD\init.lua'
no file 'C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\RunTime\LuaScripts\RSTD.lua'
no file 'C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\RunTime\..\Clients\LuaModules\LuaSocket\RSTD.lua'
no file '.\RSTD.dll'
no file 'C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\RunTime\RSTD.dll'
no file 'C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\RunTime\loadall.dll'
no file 'C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\RunTime\..\Clients\LuaModules\RSTD.dll'
no file 'C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\RunTime\..\Clients\LuaModules\LuaSocket\RSTD.dll'
***Script completed successfully.***

This is the result I get when I press "Run" while executing mmWave. How can I resolve this?

  • 感谢您对TI产品的关注!
    关于你的咨询,RSTD是一个用于实时显示数据和控制信息的工具。
    如果MMWave Studio软件无法加载RSTD模块Failed to load RSTD module,
    这可能意味着RSTD模块没有正确安装或者存在兼容性问题。

    确认下RSTD模块是否已经正确安装。如果没有安装或安装不正确,
    请按照MMWave Studio的说明进行安装。

    确认你的操作系统和MMWave Studio的版本是否兼容。

    查看是否有任何防火墙或安全软件阻止了RSTD模块的加载。
    或者安装是未关闭防火墙或安全软件阻止了它的安装。