Other Parts Discussed in Thread: AWR2243, AWR1843, IWR1843, IWR1843BOOST, AWR2944, DCA1000EVM
请问AWR2243级联板如何实现硬件触发,我知道AWR1843可以通过将一个连接sync_in引脚的零欧电阻去掉,即可实现hardware triiger,AWR2243如何实现硬件触发呢,也需要通过焊接去掉一个零欧电阻吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问AWR2243级联板如何实现硬件触发,我知道AWR1843可以通过将一个连接sync_in引脚的零欧电阻去掉,即可实现hardware triiger,AWR2243如何实现硬件触发呢,也需要通过焊接去掉一个零欧电阻吗?
感谢您对TI产品的关注!
关于你的咨询,要在AWR2243级联板上实现硬件触发,需要进行以下步骤:
将触发信号输入到 sync_in 引脚。
在 framecfg 中设置帧数(例如,设置为10),并选择硬件触发模式。当外部输入同步脉冲时,芯片将发送设定数量的帧。
你可以看看下面2个相似问题咨询的帖子。
e2echina.ti.com/.../awr2243-awr2243
e2echina.ti.com/.../mmwcas-rf-evm-awr2243
您好,该链接中提到了无法对2243级联板的maste radar进行触发:
https://e2echina.ti.com/support/sensors/f/sensors-forum/286096/awr2243-awr2243
但是下面这个链接又提到了可以进行硬件触发:
https://e2echina.ti.com/support/sensors/f/sensors-forum/794699/mmwcas-rf-evm-awr2243
按照我的理解。只有硬件触发了awr2243 master才是真正地硬件触发,所以到底能否实现硬件触发呢?
另外,如何获取AWR2243级联板的供电标准,接线方式之类的教程,需要参考哪个手册呢?
1. 我阅读了这两个pdf,看到了如下图的内容,确实说是可以通过外部脉冲实现硬件触发的:

但是之前我在使用IWR1843的时候得知需要移除IWR1843Boost上的R62才可以实现硬件触发,如下图所示:

所以我想知道:AWR2944 Cascade是否也需要类似的操作呢?
2. 我从你给我的这两个文档中得知,MMWCAS-RF-EVM级联板需要一个5V的电源适配器,对吗?
请问给MMWCAS-DSP-EVM的供电应该是多少呢,我主要想要了解的其实是我在使用MMWCAS-RF-EVM+MMWCAS-DSP-EVM这套系统时,应该如何接线。就像之前用IWR1843BOOST+DCA1000EVM时,是通过给雷达5V供电,DCA1000通过雷达供电这样的方式。