This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP100: 传感器论坛

Part Number: TMP100


您好, 我在产品中用到了这颗器件,I2C总线上挂载了ESD二极管,ESD二极管型号为LESDA6V1LT1G。在产品寄到客户那里前,是做过高低温循环的(90度-25度),直到测试结束,I2C通信均正常,我们也确定产品是正常可以出货的,就进行了打包装箱,运输给客户,客户拿到产品后,第一次通电就功能异常,我们售后现场调试也异常,最后将产品寄回来查找问题,最终定位到是这颗芯片损坏;损坏导致的现象是I2C总线的SCK和SDA信号异常,不是完整的方波,是畸形的波形,低电平不能到0V(低电平电压大致在2.5V左右),信号边沿有很大的过冲,但空闲时是3.3V电压。这条I2C总线上的器件ESD防护二极管没有损坏。此芯片是焊接在PCB板上的,整个产品做了密封灌胶。请问这颗芯片是遇到了什么情况导致了此现象? 谢谢!