This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP112-Q1: ALERT觸發後,並且清除ALERT之後要如何在回到默認狀態

Part Number: TMP112-Q1


Hi 您好,

1.我在初始化的操作對配置寄存器做了如下的操作:

BYTE 1: 0x62
BYTE 2: 0x80

這個主要是針對BYTE1  D1 名稱為TM的這個Bit操作成中斷模式..

2.接著我對高溫跟低溫寄存器進行了溫度參數的配置:

高溫寄存器:

BYTE 1: 0x32
BYTE 2: 0x00

低溫寄存器:

BYTE 1: 0xE7
BYTE 2: 0x00

3.當我的環境溫度超過高溫寄存器的數值(50度)時,ALERT Pin腳觸發變成 active low時,我去讀取溫度寄存器做清除的動作,ALERT pin會變成active high.

4.這時候當我的環境溫度下降到正常溫度後(小於高溫寄存器),環境溫度再次高於高溫寄存器時,ALERT腳位卻不會觸發成 active low.

請問是正常嗎?又或是我哪邊要再設定呢?

BRs,

Danny