This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: 雷达测量静止物体,相位产生周期性偏移

Part Number: AWR2243


1.利用2243进行测量,并未利用角反

1.1 问题描述

雷达对静止目标(强目标和弱目标)进行相位监控时,在雷达和目标都保持静止的情况下,距离较远。理论情况下,目标相位应该是固定不变的,有波动的话,波动也是较小的。实际情况,在长时间监控下,目标相位会发生慢变,一个小时波动约150度左右。具体情况如下所示。

1.2 场景

对静止大楼进行相位监测,雷达也是固定静止的,选取能量高的峰值点,每一帧的时间为40ms,总共监控1小时,相位变化情况如下图所示。

目标①:右图为相位目标变化情况,横轴为帧数,纵轴为相位。

目标②:右图为相位目标变化情况,横轴为帧数,纵轴为相位。

2. 利用2944测量,使用角反

2.1 问题描述

本节利用2944雷达进行测量,雷达设置为单发四收,目标距离15m处,测量半小时左右,目标位置设置角反,同样产生相位周期性偏移,但相位偏移量较小,五分钟内最大相位差为0.35,忽略明显的抖动部分,

相位差较小的原因认为在于使用角反辅助。

2.2 场景

        目标①:右图纵轴为相位,横轴为时间(min)