This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944: AWR2944无法启动问题

Part Number: AWR2944


TI专家们:

       你们好!我们最近遇到了一个问题,就是我们使用了AWR2944核心板,C16(MSS_UARTA_TX)这个引脚。

我们初始SOP4:0配置,使用10K电阻下拉到地。

另外,我们使用到CAN通信,所以将这个引脚通过0R电阻连接到CAN收发器(TJA1051)。大概在9月底,我们正常使用,发现雷达上电后可以正常启动,没有问题;在最近几天调试,发现同一个板子,雷达上电无法正常启动。

分析排查之后,发现C16这个引脚,如果拆掉0R电阻,断开C16和CAN收发器的连接,则雷达启动没有问题。

请问,这个雷达调试工具及相关的库文件,是否有更新?另外这个引脚配置成什么状态,才不会导致雷达无法启动?无法启动的原因是什么?

以上问题,请帮忙解答一下。

除此之外,对于雷达供电,期待的纹波允许值是什么范围?需额外注意那几个电源引脚供电?