This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我使用Hardware Trigger触发AWR1843BOOST(其他配置均为默认)发现并没有成功触发,Output中显示如下信息。在其他配置不变的情况下,使用Software Trigger则可以成功触发。之前也使用过Hardware Trigger,没有出现这种问题。
Hardware Trigger触发时,Output信息:
[20:54:58] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
[20:54:58] [RadarAPI]: Sending start_record command to DCA1000
[20:54:59] [RadarAPI]: ar1.StartFrame()
[20:54:59] [RadarAPI]: Status: Passed
[20:54:59] Frame start async event received!
[20:54:59] [RadarAPI]: Frame Ended
[20:55:28] [RadarAPI]:
[20:55:28] [RadarAPI]:
[20:55:28] Start Record command : Success
[20:55:28]
[20:55:28] No LVDS data
[20:55:28]
[20:55:28] Record stop is done successfully
请问如何解决这个情况?