This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC7201-ZAX-EVM: Connection Wrong

Part Number: TDC7201-ZAX-EVM
Other Parts Discussed in Thread: TDC7200, TDC7201

Hello, dear engineer, I am trying to drive TDC7201 with FPGA. I wrote the program according to the few TDC7200 routines, but when I connected TDC and FPGA, I couldn't drive it and there was no response. I connected ENABLE, SCLK, GND, INTB1, VDD, CSB1, DOUT1, DIN. I made sure that I should choose mode 1 of TDC1, and I didn't connect them wrong. That blog can also drive it, because I have successfully driven it with MSP myself. When connecting with MSP, EXT_CLOCK was not connected, so I didn't connect CLOCK. I would like to ask if the driving failure is due to this reason. If not, I would like to hear your thoughts.The blog address is blog.csdn.net/.../121719751