This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
如果更换IC后正常,说明IC损坏。
LMT87的外围电路很简单,建议是在VDD和GND之间加旁路电容。
根据数据手册Table 4, 如果输出端电容> 1100 pF,建议串联电阻(Table 4)。
您电路中采用的是0.1uf, 建议串联1.5 kΩ电阻。
具有 AB 类输出的 LMT87 2.7V、SC70/TO-92/TO-92S 模拟温度传感器 datasheet (Rev. E)