你好,
在使用HDC3020DEFR经过 532小时的双85测试(85度温度,85%RH)后,有部分HDC3020DEFR的湿度值偏差非常大(如标识的橙色表格),请帮忙分析一下是什么原因造成的呢?谢谢!

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
在使用HDC3020DEFR经过 532小时的双85测试(85度温度,85%RH)后,有部分HDC3020DEFR的湿度值偏差非常大(如标识的橙色表格),请帮忙分析一下是什么原因造成的呢?谢谢!

您好,
虽然压力测试(如85C/85%RH)通常是为了测试传感器的可靠性,但需要注意的是湿度传感器有特殊的存储和处理指南。 右侧传感器有一个开放型腔,可将聚合物暴露在空气中,暴露的聚合物可能会受到极端条件(超过数据表规格的条件)的影响,包括85C/85%RH,从而导致相对湿度测量发生变化。 在这种情况下,选择超出数据表规格的相对湿度百分比和温度不能作为现场传感器性能的可靠预测指标。
请参阅HDC3020数据表第6.3和8.4.3.4节以及白皮书85°C/85% RH加速寿命测试对湿度传感器的影响。