This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3006: OPT3006 不同批次IIC设备地址不一样,于SPEC不符

Part Number: OPT3006


OPT3006如下批次出现批次性设备IIC地址与SPEC不符,如下问题麻烦TI 同仁回复确认

1.查询到code 2233+5批次Ti有出现过召回历史,麻烦确认召回原因,召回是否涉及到code 2234+5批次,还有哪些批次被召回过

2.不同批次,地址不一致。是否有区分?后续TI打算怎么做区分?

3.OPT3006还有哪些常见问题,麻烦列出

4.我们将code 2234+5批次OPT3006的IIC地址由0X44变到0X45,可以正常通讯了,现推荐终端(baxter)驱动中的IIC地址做相应调整,麻烦确认对客户端软件调试是否有影响,OPT3006自身功能是否有影响。

5.麻烦确认OPT3006的IIC地址为什么会与spec不符,根本原因是什么?

  • 您好,   

    在此澄清一下,设备没有响应地址0x44和地址0x45?这是否正确?

    是否还验证设备仅响应此I2C地址? 是否尝试使用GND,VDD,SDA和SCL信号来查看I2C是否可更换?

    我们需要在内部检查此日期代码的历史记录,看看过去是否有任何其他问题。

    I2C地址的差异不应对设备功能产生影响,但我会对此进行检查并尽快解答您的疑虑。