Other Parts Discussed in Thread: DCA1000EVM
IWRL1432BOOST-BSD 适配电源为多少?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
IWRL1432BOOST-BSD 适配电源请参考以下资料,
www.ti.com.cn/.../swru619.pdf
“2.5 Connectors”和“2.15.2 Higher Power Demanding Applications”
Most of the EVM can be operated with a single USB cable itself. For higher power consumption applications
where a single USB-port cannot supply the power needed, use an external 12 V/2A or higher power adapter.
关于DCA1000EVM适配电源请参考以下资料,
https://www.ti.com.cn/cn/lit/ml/spruik7/spruik7.pdf#page=2
The DCA1000 and the xWR EVM are powered with 5-V, 2.5-A supplies.
www.ti.com.cn/.../spruij4a.pdf
“Power Connections”部分