This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00663: VCC_laser

Part Number: TIDA-00663
Other Parts Discussed in Thread: OPA857

上电后,VCC_laser信号受电路影响存在周期性波动(会影响到接收部分OPA857的输入吗)。PCB上选择的SPLPL90_3方案。去掉MOSFET后会变得较为平稳。

  • 您好

    VCC_laser信号波动对OPA857输入的影响

    1. 信号波动情况

    VCC_laser信号在上电后存在周期性波动,这可能是由于电路中的某些元件或设计导致的。当去掉MOSFET后,信号变得较为平稳,这表明MOSFET可能是引起波动的一个因素。

    2. 对OPA857输入的影响

    • 潜在影响‌:VCC_laser信号的波动可能会通过电源或地线等路径耦合到OPA857的输入端,从而影响其正常工作。特别是如果波动频率与OPA857的输入频率范围相近时,更容易产生干扰。
    • 具体表现‌:干扰可能导致OPA857输出信号的失真、噪声增加或性能下降等。这会影响整个接收部分的灵敏度和准确性。

    3. 建议措施

    • 优化电路设计‌:重新审查电路设计,特别是与VCC_laser相关的部分,确保没有不必要的元件或设计缺陷导致信号波动。
    • 增加滤波措施‌:在VCC_laser信号线上增加适当的滤波元件,如电容、电感等,以减小波动。

    综上所述,VCC_laser信号的波动确实有可能对OPA857的输入产生影响,需要采取相应的措施来确保电路的稳定性和性能。