This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944: AWR2944

Part Number: AWR2944


你好

在cli模块设置localmax阈值和cafar阈值后,最终经过如下转换输入到HWA中使用,请问转换是什么意思,有没有文档介绍。

Local Max:

 /* 2D maximum value offset */
#define CONST_LOG2_10 (3.3219f)
scratchVal = round((float)(obj->cfarAzimFFTCfg.localMaxCfg.azimThreshold)* ((1.0f/20.0f) * CONST_LOG2_10 * 2048.0f));
obj->dopplerAzimHwaCommonConfig.advStatConfig.max2DoffsetDim1 = -scratchVal;
scratchVal = round((float)(obj->cfarAzimFFTCfg.localMaxCfg.dopplerThreshold)* ((1.0f/20.0f) * CONST_LOG2_10 * 2048.0f));
obj->dopplerAzimHwaCommonConfig.advStatConfig.max2DoffsetDim2 = -scratchVal;

Range Cfar:

static uint16_t Mmw_convertRangeCfarToThresh(uint16_t codedCfarVal, uint8_t numBands)
{
uint16_t linearVal;
float dbVal, linVal;
uint32_t defaultScaling = 1 << 11;
float additionalScaling = numBands / (float)(1 << mathUtils_ceilLog2(numBands));

/* dbVal is a float value from 0-100dB. It needs to
be converted to linear scale..
First, recover float dbVal that was encoded in CLI. */
dbVal = (float)(codedCfarVal / MMW_CFAR_THRESHOLD_ENCODING_FACTOR);

/* Now convert it to linear value */
linVal = (uint32_t)(log2f(pow(10, (float)dbVal/20.0)) * additionalScaling * defaultScaling + 0.5);

linearVal = (uint16_t) linVal;
return (linearVal);
}

Doppler Cfar:

#define CONST_LOG2_10 (3.3219)
static uint16_t Mmw_convertDopplerCfarToThresh(uint16_t codedCfarVal)
{
uint16_t linearVal;
float dbVal, linVal;

/* dbVal is a float value from 0-100dB. It needs to
be converted to linear scale..
First, recover float dbVal that was encoded in CLI. */
dbVal = (float)(codedCfarVal / MMW_CFAR_THRESHOLD_ENCODING_FACTOR);

/* Now convert it to linear value */
linVal = (uint32_t)(dbVal/20.0 * CONST_LOG2_10 * 2048.0);

linearVal = (uint16_t) linVal;
return (linearVal);
}

  • 您好,

    阈值以 dB 为单位、以 Q11格式从 log10转换为 log2。

    20*log10(val) = dBVal

    log10(val^20) = dBVal

    10^dBVal = val^20

    log2(10^dBVal) = log2(val^20)

    log2(10^dBVal) = 20*log2(val)

    1/20 * log2(10^dBVal) = log2(val)

    log2(10^(dBVal/20)) = log2(val) ->此公式用于演示

    HWA CFAR 阈值应采用此格式配置。