dears,
我的客户在测试IWRL6432的EVM板, 目前已能正常工作且距离反馈OK,但有关手势的部分在测试过程中出现了一些问题:
①在使用雷达工具箱配置中(CCS途径安装,visualizer直接运行),DEMO选择未找到示例中的IWRL6432 Gesture Recognition,只能使用Gesture Recognition


②手势信号识别不灵敏的情况(存在波形变化,但无手势信号输出)(距离50cm)
③power usage存在突变的情况,且请确认这是否正常(笔记本电池已设置为最佳性能)
INFO [gui_core.py:251] CLI COM Port found: COM7 INFO [gui_core.py:260] Data COM Port found: COM8 INFO [gui_parser.py:292] Connected (one port) with baud rate 1250000 b'channelCfg 7 3 0\n' b'\n' b'Done\r\n' b'\n' b'mmwDemo:/>chirpComnCfg 21 0 0 128 1 34 0\n' b'\n' b'Done\r\n' b'\n' b'mmwDemo:/>chirpTimingCfg 8 20 0 102.98 59\n' b'\n' b'Done\r\n' b'\n' b'mmwDemo:/>frameCfg 2 0 200 128 35 0\n' b'\n' b'Done\r\n' b'\n' b'mmwDemo:/>sigProcChainCfg2 32 32 1 1.35 2.25 25 8 1 1\n' b'\n' b'Done\r\n' b'\n' b'mmwDemo:/>adcDataSource 0 C:/ti/mmwave_lp_sdk/examples/datapath/common/testBench/gesture_recognition_adc_data/radar_data_6432_100framesS.bin\n' b'\n' b'Done\r\n' b'\n' b'mmwDemo:/>adcLogging 0\n' b'\n' b'Done\r\n' b'\n' b'mmwDemo:/>cfarMinorMotionCfg 2 8 3 3 8.0 1\n' b'\n' b'Done\r\n' b'\n' b'mmwDemo:/>boardTiltAngle 0\n' b'\n' b'Done\r\n' b'\n' b'mmwDemo:/>pointCloudEnable 0\n' b'\n' b'Done\r\n' b'\n' b'mmwDemo:/>guiMonSel 0 1 0 1\n' b'\n' b'Done\r\n' b'\n' b'mmwDemo:/>presenceDetectCfg 1 1200 2000 10\n' b'\n' b'Done\r\n' b'\n' b'mmwDemo:/>lowPowerCfg 1\n' b'\n' b'Done\r\n' b'\n' b'mmwDemo:/>factoryCalibCfg 1 0 40 0 0x1ff000\n' b'\n' b'Done\r\n' b'\n' b'mmwDemo:/>sensorStart 0 0 0 0\n' b'\n' b'Done\r\n' b'\n' QWindowsWindow::setGeometry: Unable to set geometry 1366x743+0+23 (frame: 1382x782-8-8) on QWidgetWindow/"WindowClassWindow" on "\\.\DISPLAY1". Resulting geometry: 1366x705+0+23 (frame: 1382x744-8-8) margins: 8, 31, 8, 8 minimum size: 1120x743 MINMAXINFO maxSize=0,0 maxpos=0,0 mintrack=1136,782 maxtrack=0,0)
客户使用的两台测试设备均为win10笔记本且结果一致,附件为visualizer测试问题现象与代码,请帮忙指导一下应该如何解决这几个问题。
谢谢!