This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843BOOST: IWR1843BOOST数据传输

Part Number: IWR1843BOOST

  你好,我想使用USB转TTL线直接连接评估版的UART串口,请问是连接到评估版J6的4、5、7Pin端口上吗,SPO/1/2需要更改到什么模式吗?还是在别的端口可以连接UART串口,麻烦给解答一下吧

  • 你好,

    SPO/1/2需要更改到什么模式吗?

    SOP是控制芯片的工作模式的,你的这个数据传输需要芯片工作在functional mode吗?

    默认uar是连在XDS110的M4芯片上的,你需要调整板上卡关切换到其他接口上,具体请参考IWR1843BOOST原理图。

    Thanks,

    Chris