This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: awr1843 BOOST

Part Number: AWR1843BOOST
Other Parts Discussed in Thread: AWR1843, SYSBIOS

我现在在用AWR1843 BOOST 与电脑进行串口通信,设置的单发单收,帧周期为50ms,每帧发射一个chirp,波特率调到3125000,按理来说,一秒应该接收到20个chirp,但我实际每秒只能接收到4个chirp,如何才能解决这个问题,以下是我CCS中的相关代码:

/*
* ======== main.c ========
*/

#include <stdint.h>
#include <stdlib.h>
#include <stddef.h>
#include <string.h>
#include <stdio.h>
#include <math.h>

/* BIOS/XDC Include Files. */
#include <xdc/std.h>
#include <xdc/cfg/global.h>
#include <xdc/runtime/IHeap.h>
#include <xdc/runtime/System.h>
#include <xdc/runtime/Error.h>
#include <xdc/runtime/Memory.h>
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/knl/Event.h>
#include <ti/sysbios/knl/Semaphore.h>
#include <ti/sysbios/knl/Clock.h>
#include <ti/sysbios/heaps/HeapBuf.h>
#include <ti/sysbios/heaps/HeapMem.h>
#include <ti/sysbios/knl/Event.h>
#include <ti/sysbios/family/arm/v7a/Pmu.h>
#include <ti/sysbios/family/arm/v7r/vim/Hwi.h>

/* mmWave SDK Include Files: */
#include <ti/common/sys_common.h>
#include <ti/drivers/soc/soc.h>
#include <ti/drivers/esm/esm.h>
#include <ti/drivers/crc/crc.h>
#include <ti/drivers/uart/UART.h>
#include <ti/drivers/gpio/gpio.h>
#include <ti/drivers/pinmux/include/pinmux_xwr18xx.h>
#include <ti/drivers/pinmux/pinmux.h>
#include <ti/drivers/osal/DebugP.h>
#include <ti/drivers/adcbuf/ADCBuf.h>
#include <ti/control/mmwave/mmwave.h>

#include "mss_adcdata.h"
#include "signalDesign.h"

#pragma DATA_ALIGN(gAdcdataMSSMCB, 16)
Adcdata_MSS_MCB gAdcdataMSSMCB;

/**
* @b Description
* @n
* This is the callback function registered with the ADC Driver which is invoked
* when a chirp is available. This is executed in the ISR context.
*
* @param[in] arg
* Application registered argument
*
* @retval
* Not Applicable.
*/
static void Adcdata_MSS_chirpIntCallback(uintptr_t arg)
{
gAdcdataMSSMCB.chirpInt++;
if(gAdcdataMSSMCB.chirpInt == 1)
{
gAdcdataMSSMCB.frameflag = ~gAdcdataMSSMCB.frameflag;
gAdcdataMSSMCB.chirpInt = 0;
Semaphore_post(gAdcdataMSSMCB.uartSendSemHandle);
}
}

/**
* @b Description
* @n
* This is the callback function registered with the ADC Driver which is invoked
* when a frame is started. This is executed in the ISR context.
*
* @param[in] arg
* Application registered argument
*
* @retval
* Not Applicable.
*/
static void Adcdata_MSS_frameStartIntCallback(uintptr_t arg)
{

}

/**
* @b Description
* @n
* This is the task which provides an execution context for
* the mmWave control module.
*
* @param[in] arg0
* Argument0 with which the task was created
* @param[in] arg1
* Argument1 with which the task was created
*
* @retval
* Not Applicable.
*/
static void Adcdata_MSS_mmWaveCtrlTask (UArg arg0, UArg arg1)
{
int32_t errCode;

while (1)
{
/* Execute the mmWave control module: */
if (MMWave_execute (gAdcdataMSSMCB.ctrlHandle, &errCode) < 0)
{
System_printf ("Error: mmWave control execution failed [Error code %d]\n", errCode);
}
}
}


/*
*
*
*
* */
static void Adcdata_MSS_UartSendTask (UArg arg0, UArg arg1)
{
gAdcdataMSSMCB.head.messageHead[0] = 0x11;
gAdcdataMSSMCB.head.messageHead[1] = 0x22;
gAdcdataMSSMCB.head.messageHead[2] = 0x33;
gAdcdataMSSMCB.head.messageHead[3] = 0x22;
gAdcdataMSSMCB.head.messageHead[4] = 0x11;
while (1)
{
Semaphore_pend(gAdcdataMSSMCB.uartSendSemHandle, BIOS_WAIT_FOREVER);

UART_writePolling (gAdcdataMSSMCB.loggingUartHandle,
(uint8_t*)&gAdcdataMSSMCB.head,
sizeof(Adcdata_MessageHeader));

UART_writePolling (gAdcdataMSSMCB.loggingUartHandle,
(uint8_t*)gAdcdataMSSMCB.adcDataBuf,
PROFILE_ADC_SAMPLE_VAL*4);
}
}

/**
* @b Description
* @n
* Registered event function which is invoked when an event from the
* BSS is received.
*
* @param[in] msgId
* Message Identifier
* @param[in] sbId
* Subblock identifier
* @param[in] sbLen
* Length of the subblock
* @param[in] payload
* Pointer to the payload buffer
*
* @retval
* Always returns 0 [Continue passing the event to the peer domain]
*/
static int32_t Adcdata_MSS_eventFxn(uint16_t msgId, uint16_t sbId, uint16_t sbLen, uint8_t *payload)
{
uint16_t asyncSB = RL_GET_SBID_FROM_UNIQ_SBID(sbId);

/* Process the received message: */
switch (msgId)
{
case RL_RF_ASYNC_EVENT_MSG:
{
/* Received Asychronous Message: */
switch (asyncSB)
{
case RL_RF_AE_CPUFAULT_SB:
{
/* Post event to datapath task notify BSS events */
//Event_post(gMrrMSSMCB.eventHandle, MMWDEMO_BSS_CPUFAULT_EVT);
break;
}
case RL_RF_AE_ESMFAULT_SB:
{
/* Post event to datapath task notify BSS events */
//Event_post(gMrrMSSMCB.eventHandle, MMWDEMO_BSS_ESMFAULT_EVT);
break;
}
case RL_RF_AE_INITCALIBSTATUS_SB:
{
/* This event should be handled by mmwave internally, ignore the event here */
break;
}
case RL_RF_AE_FRAME_TRIGGER_RDY_SB:
{
break;
}
case RL_RF_AE_MON_TIMING_FAIL_REPORT_SB:
{
break;
}
case RL_RF_AE_RUN_TIME_CALIB_REPORT_SB:
{
break;
}
default:
{
System_printf ("Error: Asynchronous Event SB Id %d not handled\n", asyncSB);
break;
}
}
break;
}
default:
{
System_printf ("Error: Asynchronous message %d is NOT handled\n", msgId);
break;
}
}
return 0;
}


/**
* @b Description
* @n
* Function to configure ADCBUF driver based on CLI inputs.
* @param[out] numRxChannels Number of receive channels.
*
* @retval
* Not Applicable.
*/
static int32_t Adcdata_ADCbufConfig()
{
ADCBuf_dataFormat dataFormat;
ADCBuf_RxChanConf rxChanConf;
int32_t retVal;
uint8_t channel;
uint8_t adcFmt;
uint8_t chInterleave;
uint8_t sampleInterleave;
uint32_t chirpThreshold;
uint32_t rxChanMask = 0xF; /* All channels are enabled. */
uint32_t offset;

adcFmt = 0; /* Complex mode */
chInterleave = 1; /* Channel interleave mode is 1. i.e. no interleaving */
sampleInterleave = 1; /* switch to Q first then I. //Sample Interleave mode is I first then Q */
chirpThreshold = 1;

/* Divide the 32 kB ADC buffer into 4 parts. Assign each to one channel */
offset = PROFILE_ADC_SAMPLE_VAL*sizeof(cmplx16ImRe_t);

/*****************************************************************************
* Data path :: ADCBUF driver Configuration
*****************************************************************************/

/* Populate data format from configuration */
dataFormat.adcOutFormat = adcFmt;
dataFormat.channelInterleave = chInterleave;
dataFormat.sampleInterleave = sampleInterleave;

/* Disable all ADCBuf channels */
if ((retVal = ADCBuf_control(gAdcdataMSSMCB.adcBufHandle,
ADCBufMMWave_CMD_CHANNEL_DISABLE,
(void *) &rxChanMask)) < 0)
{
return retVal;
}

retVal = ADCBuf_control(gAdcdataMSSMCB.adcBufHandle,
ADCBufMMWave_CMD_CONF_DATA_FORMAT,
(void *) &dataFormat);
if (retVal < 0)
{
return -1;
}

memset((void*) &rxChanConf, 0, sizeof(ADCBuf_RxChanConf));

/* Enable all Rx Channels */
for (channel = 0; channel < SYS_COMMON_NUM_RX_CHANNEL; channel++)
{
if( RX_CHANNEL_1_ENABLE & ( 0x1U << channel ))
{
/* Populate the receive channel configuration: */
rxChanConf.channel = channel;
retVal = ADCBuf_control(gAdcdataMSSMCB.adcBufHandle,
ADCBufMMWave_CMD_CHANNEL_ENABLE,
(void *) &rxChanConf);

if (retVal < 0)
{
return -1;
}

rxChanConf.offset += offset;
}
}

/* Set ping/pong chirp threshold: */
retVal = ADCBuf_control(gAdcdataMSSMCB.adcBufHandle,
ADCBufMMWave_CMD_SET_PING_CHIRP_THRESHHOLD,
(void *) &chirpThreshold);
if (retVal < 0)
{
return -1;
}
retVal = ADCBuf_control(gAdcdataMSSMCB.adcBufHandle,
ADCBufMMWave_CMD_SET_PONG_CHIRP_THRESHHOLD,
(void *) &chirpThreshold);
if (retVal < 0)
{
return -1;
}

return 0;
}

static void InitAdcBufDriver()
{
{
ADCBuf_Params adcBufParams;

ADCBuf_init();
/*****************************************************************************
* Open ADCBUF driver:
*****************************************************************************/
ADCBuf_Params_init(&adcBufParams);
adcBufParams.chirpThresholdPing = 5;
adcBufParams.chirpThresholdPong = 5;
adcBufParams.continousMode = 0;
adcBufParams.socHandle = gAdcdataMSSMCB.socHandle;
/* Open ADCBUF driver */
gAdcdataMSSMCB.adcBufHandle = ADCBuf_open(0, &adcBufParams);
if (gAdcdataMSSMCB.adcBufHandle == NULL)
{
System_printf("Error: Unable to open the ADCBUF driver\n");
return;
}
Adcdata_ADCbufConfig();
}
return;
}

static void InitDriverTask (UArg arg0, UArg arg1)
{
int32_t errCode;
MMWave_InitCfg initCfg;
UART_Params uartParams;
Task_Params taskParams;
SOC_SysIntListenerCfg listenerCfg;
Semaphore_Params semParams;

//Debug Message:
System_printf("Debug: Launched the Initialization Task\n");

//PINMUX mapping
Pinmux_Set_OverrideCtrl(SOC_XWR18XX_PINN5_PADBE, PINMUX_OUTEN_RETAIN_HW_CTRL, PINMUX_INPEN_RETAIN_HW_CTRL);
Pinmux_Set_FuncSel(SOC_XWR18XX_PINN5_PADBE, SOC_XWR18XX_PINN5_PADBE_MSS_UARTA_TX);
Pinmux_Set_OverrideCtrl(SOC_XWR18XX_PINN4_PADBD, PINMUX_OUTEN_RETAIN_HW_CTRL, PINMUX_INPEN_RETAIN_HW_CTRL);
Pinmux_Set_FuncSel(SOC_XWR18XX_PINN4_PADBD, SOC_XWR18XX_PINN4_PADBD_MSS_UARTA_RX);

/* Setup the PINMUX to bring out the UART-3 */
Pinmux_Set_OverrideCtrl(SOC_XWR18XX_PINF14_PADAJ, PINMUX_OUTEN_RETAIN_HW_CTRL, PINMUX_INPEN_RETAIN_HW_CTRL);
Pinmux_Set_FuncSel(SOC_XWR18XX_PINF14_PADAJ, SOC_XWR18XX_PINF14_PADAJ_MSS_UARTB_TX);

/* Initialize the UART */
UART_init();

/* Initialize the GPIO */
GPIO_init();

/* Initialize the Mailbox*/
Mailbox_init(MAILBOX_TYPE_MSS);

/* Open the UART*/
UART_Params_init(&uartParams);
uartParams.clockFrequency = MSS_SYS_VCLK;
uartParams.baudRate = 115200;
uartParams.isPinMuxDone = 1;

/* Open the Command UART Instance */
gAdcdataMSSMCB.commandUartHandle = UART_open(0, &uartParams);
if (gAdcdataMSSMCB.commandUartHandle == NULL)
{
System_printf("Error: Unable to open the Command UART Instance\n");
return;
}

/* Setup the default UART Parameters */
UART_Params_init(&uartParams);
uartParams.writeDataMode = UART_DATA_BINARY;
uartParams.readDataMode = UART_DATA_BINARY;
uartParams.clockFrequency = MSS_SYS_VCLK;
uartParams.baudRate = 3125000;
uartParams.isPinMuxDone = 1U;

/* Open the Logging UART Instance: */
gAdcdataMSSMCB.loggingUartHandle = UART_open(1, &uartParams);
if (gAdcdataMSSMCB.loggingUartHandle == NULL)
{
System_printf("Error: MMWDemoMSS Unable to open the Logging UART Instance\n");
return;
}
/* Initialize the ADCBuf*/
InitAdcBufDriver();
gAdcdataMSSMCB.adcDataBuf = (cmplx16ImRe_t *)SOC_XWR18XX_MSS_ADCBUF_BASE_ADDRESS;

System_printf("Debug: ADCBuf Initialization\n");

/* Register Chirp Available Listener */
memset ((void*)&listenerCfg, 0, sizeof(SOC_SysIntListenerCfg));
listenerCfg.systemInterrupt = SOC_XWR18XX_MSS_CHIRP_AVAIL_IRQ;
listenerCfg.listenerFxn = Adcdata_MSS_chirpIntCallback;
listenerCfg.arg = 0;
gAdcdataMSSMCB.chirpIntHandle = SOC_registerSysIntListener (gAdcdataMSSMCB.socHandle, &listenerCfg, &errCode);
if (gAdcdataMSSMCB.chirpIntHandle == NULL)
{
System_printf ("Error: Unable to register the Chirp Available Listener [Error code %d]\n", errCode);
return;
}

/* Register Frame Start Listener */
memset ((void*)&listenerCfg, 0, sizeof(SOC_SysIntListenerCfg));
listenerCfg.systemInterrupt = SOC_XWR18XX_MSS_FRAME_START_INT;
listenerCfg.listenerFxn = Adcdata_MSS_frameStartIntCallback;
listenerCfg.arg = 0;
gAdcdataMSSMCB.frameStartIntHandle = SOC_registerSysIntListener (gAdcdataMSSMCB.socHandle, &listenerCfg, &errCode);

if (gAdcdataMSSMCB.frameStartIntHandle == NULL)
{
System_printf("Error: Unable to register the Frame start Listener [Error code %d]\n", errCode);
return ;
}
System_printf ("Debug: frame and chirp interrupt initialized\n");

/* Initialize the mmWave module*/
memset ((void *)&initCfg, 0, sizeof(MMWave_InitCfg));

initCfg.domain = MMWave_Domain_MSS;
initCfg.socHandle = gAdcdataMSSMCB.socHandle;
initCfg.eventFxn = &Adcdata_MSS_eventFxn;
initCfg.cfgMode = MMWave_ConfigurationMode_MINIMAL;
initCfg.executionMode = MMWave_ExecutionMode_ISOLATION;
initCfg.linkCRCCfg.useCRCDriver = 1U;
initCfg.linkCRCCfg.crcChannel = CRC_Channel_CH1;

/* Initialize and setup the mmWave Control module */
gAdcdataMSSMCB.ctrlHandle = MMWave_init (&initCfg, &errCode);
if (gAdcdataMSSMCB.ctrlHandle == NULL)
{
/* Error: Unable to initialize the mmWave control module */
System_printf ("Error: mmWave Control Initialization failed [Error code %d]\n", errCode);
return;
}
System_printf ("Debug: Initialized the mmWave module\n");

while (1)
{
int32_t syncStatus;

/* Get the synchronization status: */
syncStatus = MMWave_sync (gAdcdataMSSMCB.ctrlHandle, &errCode);
if (syncStatus < 0)
{
/* Error: Unable to synchronize the mmWave control module */
System_printf ("Error: mmWave Control Synchronization failed [Error code %d]\n", errCode);
return;
}
if (syncStatus == 1)
{
/* Synchronization acheived: */
break;
}
/* Sleep and poll again: */
Task_sleep(1);
}

System_printf ("Debug: Synchronized the mmWave module\n");

/* Create a binary semaphore which is used to handle UART Send data interrupt */
Semaphore_Params_init(&semParams);
semParams.mode = Semaphore_Mode_BINARY;
gAdcdataMSSMCB.uartSendSemHandle = Semaphore_create(0, &semParams, NULL);
System_printf ("Debug: uartSendSemHandle is created\n");
/*****************************************************************************
* Launch the mmWave control execution task
* - This should have a higher priroity than any other task which uses the
* mmWave control API
*****************************************************************************/
Task_Params_init(&taskParams);
taskParams.priority = 6;
taskParams.stackSize = 3*1024;
Task_create(Adcdata_MSS_mmWaveCtrlTask, &taskParams, NULL);
System_printf ("Debug: Adcdata_MSS_mmWaveCtrlTask is created\n");

Adcdata_MSS_Start ();
/*
* Launch the Uart Send data Task
* */
Task_Params_init(&taskParams);
taskParams.priority = 4;
taskParams.stackSize = 4*1024;
Task_create(Adcdata_MSS_UartSendTask, &taskParams, NULL);
}


/*
* ======== main ========
*/
Int main()
{
Task_Params taskParams;
int32_t errCode;
SOC_Cfg socCfg;
/* Initialize the ESM: Dont clear errors as TI RTOS does it */
ESM_init(0U);

/* Initialize the global variables */
memset ((void*)&gAdcdataMSSMCB, 0, sizeof(Adcdata_MSS_MCB));

/* Initialize the SOC configuration: */
memset ((void *)&socCfg, 0, sizeof(SOC_Cfg));

/* Populate the SOC configuration: */
socCfg.clockCfg = SOC_SysClock_INIT;
socCfg.dssCfg=SOC_DSSCfg_HALT;
socCfg.mpuCfg=SOC_MPUCfg_CONFIG;
/* Initialize the SOC Module: This is done as soon as the application is started
* to ensure that the MPU is correctly configured. */
gAdcdataMSSMCB.socHandle = SOC_init (&socCfg, &errCode);
if (gAdcdataMSSMCB.socHandle == NULL)
{
System_printf ("Error: SOC Module Initialization failed [Error code %d]\n", errCode);
return -1;
}

/* Check if the SOC is a secure device */
if (SOC_isSecureDevice(gAdcdataMSSMCB.socHandle, &errCode))
{
/* Disable firewall for JTAG and LOGGER (UART) which is needed by the demo */
SOC_controlSecureFirewall(gAdcdataMSSMCB.socHandle,
(uint32_t)(SOC_SECURE_FIREWALL_JTAG | SOC_SECURE_FIREWALL_LOGGER),
SOC_SECURE_FIREWALL_DISABLE,
&errCode);
}

System_printf ("Success: SOC Module Initialization successed\n");

/* Initialize the Task Parameters. */
Task_Params_init(&taskParams);
taskParams.priority = 1;
Task_create(InitDriverTask, &taskParams, NULL);

/* Start BIOS */
BIOS_start();
return 0;
}