In the process of using opt3101, no matter how small the current is used, such as 1.4mA. When encountering objects with high reflectivity (aluminum or stainless steel), there will be a phenomenon of saturation, and the amplitude output is 65535. What can be done to reduce this phenomenon?