This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944: SPI通信中存在较大的发送间隔的问题

Part Number: AWR2944


您好,

我目前使用mmwave_mcuplus_sdk_04_07_00_01版本开发AWR2944雷达,想将out of box Demo上点云数据传输从UART替换成SPI。我发现在传输一段完整的、较长的数据时,雷达发送一段数据就会有较长的间隔,具体如下图所示,发送数据26us、空闲56us左右。

spi设置的频率未30M,在测试中一帧大概传输了16k字节的数据,传输耗时约14.9ms,相当于spi通信速率为10M。

我对SPI的设置如下:

请问发送数据的间隔是我设置的参数有问题,还是调用SPI传输接口耗时较久?