-
Remanent flux density (Br): 1.39 T
-
Diameter: 2.5 mm
-
Height: 1 mm




-
When using the Static Position Function in TIMSS, the simulation results matched those from Magpylib (as shown in Figure 1).
-
However, when using the Linear Function in TIMSS (with the sensor selected as DRV5055A1, which is consistent with the sensor we are using in our actual application), the simulation results from TIMSS did not match those from Magpylib (as shown in Figure 2).
( Compared to the simulation results obtained using the Static Position Function in TIMSS, the results are approximately 1 mT lower. )