我希望进行关于awr1843雷达的开发,希望有两个frame,一个用于远距离探测,一个用于近距离探测,就是两个frame搭配两个不同的chirp,询问一下哪个例程可以帮助到我。并且希望有.cfg文件对雷达进行配置
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
已经收到了您的案例,调查需要些时间,感谢您的耐心等待。
您可以参考中程雷达演示(https://dev.ti.com/tirex/explore/node?node=A__ACCD.YxtaQpnE9Sm3Vf20g__radar_toolbox__1AslXXD__LATEST&placeholder=true ),
该演示使用一个子帧进行高达150米的中程探测,使用一子帧进行短程探测。为此,您需要安装雷达工具箱(dev.ti.com/.../node
在这个演示中,我们不使用*.cfg文件,而*.cfg中存在的所有配置都存在于下面提到的头文件中。
在MRR演示中,配置被硬编码在位于radar_toolbox\source\ti\examples\Automotive_ADAS_and_Parking\media_range_radar\src\1843\commodan的头文件中。
如果您正在寻找支持使用*.cfg文件进行高级帧配置的演示,可以参考SDK演示。高级帧的示例配置在SDK-mmwave_SDK_03_06_00_00-LTS \packages\ti\demo\xwr18xx\mmw\profiles\profile_advanced_subframe.cfg中提供。