This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: LVDS lane和LP ADC MODE的选择对采集的数据有什么影响

Part Number: IWR1642BOOST


当我使用iwr1642boost一发一收来进行数据采集时,选择complex1x数据格式,LVDS lane选择1或2,LP ADC MODE选择Low Power mode,如果当我选择1个LVDS lane时,数据会是samples*numchirps*2*2,每隔一个数会有一个零;当我选择2个LVDS lane时,数据时samples*numchirps*2*2/2,没有零。我想问一下LVDS lane和LP ADC MODE的选择对最终采集的数据有什么影响 
接上面问题 我的数据有一半是0,假设2个lane采集的数据为512*2048(512代表Samples,2048代表NumChirp),那我用1个lane的时候,去掉一半的0,解析之后的数据应该是512*1024还是256*2048