尊敬的Ti工程师你们好,我现在利用MMWAVE-DSP-EVM与MMWAVE-RF-EVM级联配置单发单收进行数据采集,这是我修改的官方的Cascade_Configuration_MIMO脚本:
--[[ Sequence being followed A. CONFIGURATION 1. Connecting to TDA 1. Configuring Master from SOP till Channel Config 2. Configuring Slave (i) sequentially from SOP till SPI Connect. i = 1, 2, 3 3. Configuring Slaves together from F/W download till Channel Config 4. Configuring all devices together from LDO Bypass till Frame Config NOTE: Update the following in the script accordingly before running 1. metaImage F/W path on line 32 2. TDA Host Board IP Address on line 39 --]] ----------------------------------------User Constants-------------------------------------------- dev_list = {1, 2, 4, 8} -- Device map RadarDevice = {1, 0, 0, 0} -- {dev1, dev2, dev3, dev4}, 1: Enable, 0: Disable cascade_mode_list = {1, 2, 2, 2} -- 0: Single chip, 1: Master, 2: Slave -- F/W Download Path -- Uncomment the next line if you wish to pop-up a dialog box to select the firmware image file -- Otherwise, hardcode the path to the firmware metaimage below -- By default, the firmware filename is: xwr22xx_metaImage.bin -- metaImagePath = RSTD.BrowseForFile(RSTD.GetSettingsPath(), "bin", "Browse to .bin file") -- For 2243 ES1.1 devices metaImagePath = "C:\\ti\\mmwave_dfp_02_02_04_00\\firmware\\xwr22xx_metaImage.bin" -- For 2243 ES1.0 devices -- metaImagePath = "C:\\ti\\mmwave_dfp_02_02_04_00\\firmware\\xwr22xx_metaImage.bin" -- IP Address for the TDA2 Host Board -- Change this accordingly for your setup TDA_IPAddress = "192.168.33.180" -- Device map of all the devices to be enabled by TDA -- 1 - master ; 2- slave1 ; 4 - slave2 ; 8 - slave3 deviceMapOverall = RadarDevice[1] + (RadarDevice[2]*2) + (RadarDevice[3]*4) + (RadarDevice[4]*8) deviceMapSlaves = (RadarDevice[2]*2) + (RadarDevice[3]*4) + (RadarDevice[4]*8) -- Enable/Disable Test Source -- This is useful during bringup test_source_enable = 0 -- 0: Disable, 1: Enable ------------------------------------------- Sensor Configuration ------------------------------------------------ --[[ The sensor configuration consists of 3 sections: 1) Profile Configuration (common to all 4 AWR devices) 2) Chirp Configuration (unique for each AWR device - mainly because TXs to use are different for each chirp) 3) Frame Configuration (common to all 4 AWR devices, except for the trigger mode for the master) Change the values below as needed. --]] -- Profile configuration local profile_indx = 0 local start_freq = 77 -- GHz local slope = 79 -- MHz/us local idle_time = 5 -- us local adc_start_time = 6 -- us local adc_samples = 256 -- Number of samples per chirp local sample_freq = 8000 -- ksps local ramp_end_time = 40 -- us local rx_gain = 48 -- dB local tx0OutPowerBackoffCode = 0 local tx1OutPowerBackoffCode = 0 local tx2OutPowerBackoffCode = 0 local tx0PhaseShifter = 0 local tx1PhaseShifter = 0 local tx2PhaseShifter = 0 local txStartTimeUSec = 0 local hpfCornerFreq1 = 0 -- 0: 175KHz, 1: 235KHz, 2: 350KHz, 3: 700KHz local hpfCornerFreq2 = 0 -- 0: 350KHz, 1: 700KHz, 2: 1.4MHz, 3: 2.8MHz -- Frame configuration local start_chirp_tx = 0 local end_chirp_tx = 1 local nchirp_loops = 64 -- Number of chirps per frame local nframes_master = 10 -- Number of Frames for Master local nframes_slave = 10 -- Number of Frames for Slaves local Inter_Frame_Interval = 100 -- ms local trigger_delay = 0 -- us local trig_list = {1,2,2,2} -- 1: Software trigger, 2: Hardware trigger -- Note: The syntax for this API is: -- ar1.ChirpConfig_mult(RadarDeviceId, chirpStartIdx, chirpEndIdx, profileId, startFreqVar, -- freqSlopeVar, idleTimeVar, adcStartTimeVar, tx0Enable, tx1Enable, tx2Enable) function Configure_Chirps(i) if (i == 1) then -- Chirp 0 if (0 == ar1.ChirpConfig_mult(dev_list[i], 0, 0, 0, 0, 0, 0, 0, 1, 0, 0)) then WriteToLog("Device "..i.." : Chirp 0 Configuration successful\n", "green") else WriteToLog("Device "..i.." : Chirp 0 Configuration failed\n", "red") return -4 end -- Chirp 1 if (0 == ar1.ChirpConfig_mult(dev_list[i], 1, 1, 0, 0, 0, 0, 0, 1, 0, 0)) then WriteToLog("Device "..i.." : Chirp 1 Configuration successful\n", "green") else WriteToLog("Device "..i.." : Chirp 1 Configuration failed\n", "red") return -4 end end end ------------------------------ API Configuration ------------------------------------------------ -- 1. Connection to TDA. 2. Selecting Cascade/Single Chip. 3. Selecting 2-chip/4-chip WriteToLog("Setting up Studio for Cascade started..\n", "blue") if(0 == ar1.ConnectTDA(TDA_IPAddress, 5001, deviceMapOverall)) then WriteToLog("ConnectTDA Successful\n", "green") else WriteToLog("ConnectTDA Failed\n", "red") return -1 end if(0 == ar1.selectCascadeMode(1)) then WriteToLog("selectCascadeMode Successful\n", "green") else WriteToLog("selectCascadeMode Failed\n", "red") return -1 end WriteToLog("Setting up Studio for Cascade ended..\n", "blue") --Master Initialization -- SOP Mode Configuration if (0 == ar1.SOPControl_mult(1, 4)) then WriteToLog("Master : SOP Reset Successful\n", "green") else WriteToLog("Master : SOP Reset Failed\n", "red") return -1 end -- SPI Connect if (0 == ar1.PowerOn_mult(1, 0, 1000, 0, 0)) then WriteToLog("Master : SPI Connection Successful\n", "green") else WriteToLog("Master : SPI Connection Failed\n", "red") return -1 end -- Firmware Download. (SOP 4 - MetaImage) if (0 == ar1.DownloadBssFwOvSPI_mult(1, metaImagePath)) then WriteToLog("Master : FW Download Successful\n", "green") else WriteToLog("Master : FW Download Failed\n", "red") return -1 end -- RF Power Up if (0 == ar1.RfEnable_mult(1)) then WriteToLog("Master : RF Power Up Successful\n", "green") else WriteToLog("Master : RF Power Up Failed\n", "red") return -1 end -- Channel & ADC Configuration if (0 == ar1.ChanNAdcConfig_mult(1,1,0,0,1,0,0,0,2,1,0,1)) then WriteToLog("Master : Channel & ADC Configuration Successful\n", "green") else WriteToLog("Master : Channel & ADC Configuration Failed\n", "red") return -2 end -- Slaves Initialization for i=2,table.getn(RadarDevice) do local status = 0 if ((RadarDevice[1]==1) and (RadarDevice[i]==1)) then -- SOP Mode Configuration if (0 == ar1.SOPControl_mult(dev_list[i], 4)) then WriteToLog("Device "..i.." : SOP Reset Successful\n", "green") else WriteToLog("Device "..i.." : SOP Reset Failed\n", "red") return -1 end -- SPI Connect if (0 == ar1.AddDevice(dev_list[i])) then WriteToLog("Device "..i.." : SPI Connection Successful\n", "green") else WriteToLog("Device "..i.." : SPI Connection Failed\n", "red") return -1 end end end if (deviceMapSlaves ~= 0) then -- Firmware Download. (SOP 4 - MetaImage) if (0 == ar1.DownloadBssFwOvSPI_mult(deviceMapSlaves, metaImagePath)) then WriteToLog("Slaves : FW Download Successful\n", "green") else WriteToLog("Slaves : FW Download Failed\n", "red") return -1 end -- RF Power Up if (0 == ar1.RfEnable_mult(deviceMapSlaves)) then WriteToLog("Slaves : RF Power Up Successful\n", "green") else WriteToLog("Slaves : RF Power Up Failed\n", "red") return -1 end -- Channel & ADC Configuration if (0 == ar1.ChanNAdcConfig_mult(deviceMapSlaves,1,1,1,1,1,1,1,2,1,0,2)) then WriteToLog("Slaves : Channel & ADC Configuration Successful\n", "green") else WriteToLog("Slaves : Channel & ADC Configuration Failed\n", "red") return -2 end end -- All devices together -- Including this depends on the type of board being used. -- LDO configuration if (0 == ar1.RfLdoBypassConfig_mult(deviceMapOverall, 3)) then WriteToLog("LDO Bypass Successful\n", "green") else WriteToLog("LDO Bypass failed\n", "red") return -2 end -- Low Power Mode Configuration if (0 == ar1.LPModConfig_mult(deviceMapOverall,0, 0)) then WriteToLog("Low Power Mode Configuration Successful\n", "green") else WriteToLog("Low Power Mode Configuration failed\n", "red") return -2 end -- Miscellaneous Control Configuration if (0 == ar1.SetMiscConfig_mult(deviceMapOverall, 1, 0, 0, 0)) then WriteToLog("Misc Control Configuration Successful\n", "green") else WriteToLog("Misc Control Configuration failed\n", "red") return -2 end -- Edit this API to enable/disable the boot time calibration. Enabled by default. -- RF Init Calibration Configuration if (0 == ar1.RfInitCalibConfig_mult(deviceMapOverall, 1, 1, 1, 1, 1, 1, 1, 65537)) then WriteToLog("RF Init Calibration Successful\n", "green") else WriteToLog("RF Init Calibration failed\n", "red") return -2 end -- RF Init if (0 == ar1.RfInit_mult(deviceMapOverall)) then WriteToLog("RF Init Successful\n", "green") else WriteToLog("RF Init failed\n", "red") return -2 end ---------------------------Data Configuration---------------------------------- -- Data path Configuration if (0 == ar1.DataPathConfig_mult(deviceMapOverall, 0, 1, 0)) then WriteToLog("Data Path Configuration Successful\n", "green") else WriteToLog("Data Path Configuration failed\n", "red") return -3 end -- Clock Configuration if (0 == ar1.LvdsClkConfig_mult(deviceMapOverall, 1, 1)) then WriteToLog("Clock Configuration Successful\n", "green") else WriteToLog("Clock Configuration failed\n", "red") return -3 end -- CSI2 Configuration if (0 == ar1.CSI2LaneConfig_mult(deviceMapOverall, 1, 0, 2, 0, 4, 0, 5, 0, 3, 0, 0)) then WriteToLog("CSI2 Configuration Successful\n", "green") else WriteToLog("CSI2 Configuration failed\n", "red") return -3 end ----------------------------Test Source Configuration------------------------------ -- This is useful for initial bringup. -- Each device is configured with a test object at a different location. --delete ---------------------------Sensor Configuration------------------------- -- Profile Configuration if (0 == ar1.ProfileConfig_mult(deviceMapOverall, 0, start_freq, idle_time, adc_start_time, ramp_end_time, 0, 0, 0, 0, 0, 0, slope, 0, adc_samples, sample_freq, 0, 0, rx_gain)) then WriteToLog("Profile Configuration successful\n", "green") else WriteToLog("Profile Configuration failed\n", "red") return -4 end -- Chirp Configuration for i=1,table.getn(RadarDevice) do if ((RadarDevice[1]==1) and (RadarDevice[i]==1)) then Configure_Chirps(i) end end -- Enabling/ Disabling Test Source if(test_source_enable == 1) then ar1.EnableTestSource_mult(deviceMapOverall, 1) WriteToLog("Enabling Test Source Configuration successful\n", "green") end -- Frame Configuration -- Master if (0 == ar1.FrameConfig_mult(1,start_chirp_tx,end_chirp_tx,nframes_master, nchirp_loops, Inter_Frame_Interval, 0, 1)) then WriteToLog("Master : Frame Configuration successful\n", "green") else WriteToLog("Master : Frame Configuration failed\n", "red") end -- Slaves if (deviceMapSlaves ~= 0) then if (0 == ar1.FrameConfig_mult(deviceMapSlaves,start_chirp_tx,end_chirp_tx,nframes_slave, nchirp_loops, Inter_Frame_Interval, 0, 2)) then WriteToLog("Slaves : Frame Configuration successful\n", "green") else WriteToLog("Slaves : Frame Configuration failed\n", "red") end end在这份为了配置单发单收而修改后的脚本里,我做的主要改动是:
RadarDevice = {1, 0, 0, 0} -- {dev1, dev2, dev3, dev4}, 1: Enable, 0: Disable function Configure_Chirps(i) if (i == 1) then -- Chirp 0 if (0 == ar1.ChirpConfig_mult(dev_list[i], 0, 0, 0, 0, 0, 0, 0, 1, 0, 0)) then WriteToLog("Device "..i.." : Chirp 0 Configuration successful\n", "green") else WriteToLog("Device "..i.." : Chirp 0 Configuration failed\n", "red") return -4 end -- Chirp 1 if (0 == ar1.ChirpConfig_mult(dev_list[i], 1, 1, 0, 0, 0, 0, 0, 1, 0, 0)) then WriteToLog("Device "..i.." : Chirp 1 Configuration successful\n", "green") else WriteToLog("Device "..i.." : Chirp 1 Configuration failed\n", "red") return -4 end end end -- Channel & ADC Configuration if (0 == ar1.ChanNAdcConfig_mult(1,1,0,0,1,0,0,0,2,1,0,1)) then WriteToLog("Master : Channel & ADC Configuration Successful\n", "green") else WriteToLog("Master : Channel & ADC Configuration Failed\n", "red") return -2 end if (deviceMapSlaves ~= 0) then -- Firmware Download. (SOP 4 - MetaImage) if (0 == ar1.DownloadBssFwOvSPI_mult(deviceMapSlaves, metaImagePath)) then WriteToLog("Slaves : FW Download Successful\n", "green") else WriteToLog("Slaves : FW Download Failed\n", "red") return -1 end -- RF Power Up if (0 == ar1.RfEnable_mult(deviceMapSlaves)) then WriteToLog("Slaves : RF Power Up Successful\n", "green") else WriteToLog("Slaves : RF Power Up Failed\n", "red") return -1 end -- Channel & ADC Configuration if (0 == ar1.ChanNAdcConfig_mult(deviceMapSlaves,1,1,1,1,1,1,1,2,1,0,2)) then WriteToLog("Slaves : Channel & ADC Configuration Successful\n", "green") else WriteToLog("Slaves : Channel & ADC Configuration Failed\n", "red") return -2 end end ----------------------------Test Source Configuration------------------------------ -- This is useful for initial bringup. -- Each device is configured with a test object at a different location. --delete -- Slaves if (deviceMapSlaves ~= 0) then if (0 == ar1.FrameConfig_mult(deviceMapSlaves,start_chirp_tx,end_chirp_tx,nframes_slave, nchirp_loops, Inter_Frame_Interval, 0, 2)) then WriteToLog("Slaves : Frame Configuration successful\n", "green") else WriteToLog("Slaves : Frame Configuration failed\n", "red") end end然后我利用官方提供的capture脚本采集数据,但是mmwavestudio日志信息会报错:[15:31:01] Create Application Response from Capture Card timed out!!
[15:31:01] TDA ARM Failed
我想请问一下是我的配置脚本有地方没有修改正确还是说capture脚本里面也需要作一定的修改呢?