This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944: chirpCfg配置的含义

Part Number: AWR2944

您好,

我们目前按在SDK 4.6.1.2版本下开发AWR2944雷达,我对cfp配置中chirpcfg配置的第4、第5、第6个参数有些疑问。问题如下:

1. 第4、第5、第6三个参数是在每帧数据起始时生效?还是在每个chirp发射时生效?

2. 以第4个参数为例,假设profilecfg中设置的起始频率是77GHz、chirpCfg的第四个参数是1000,000,000,这个配置的意思是每次开始时起始频率会是 76GHz~78GHz之间的任意值吗?

3. 第5、第6个参数的生效方式跟第二个问题中的方式是一样的吗?

4. SDK 4.6.1.2中显示这三个参数只在 '0' 时测试过,如何确认三个参数修改生效呢?

5. 修改这三个参数会有什么风险吗?