Part Number: IWR1843BOOST
Dear TI engineers, hello!
I wrote the DataCapture.lua file as needed and used matlab to send the configuration parameters of the radar to mmwave studio through the lua script, but encountered the error as shown in the following figure.

As shown in the above figure, in the sensorconfig TAB, the profile and others have been changed according to the datacapture.lua file. However, there was a problem when setting up the TX2. I tried to change ar1.ChirpConfig(2, 2, 0, 0, 0, 0, 0, 0, 0, 1) to ar1.ChirpConfig(1,1, 0, 0, 0, 0, 0, 1), but it still didn't work. Please help me. Thank you very much.