Part Number: AWR1443BOOST
Use 2TX-4RX (two transmitters and four receivers), and check "TX0, TX2" in the “staticConfig” title.
Question 1: After completing the configuration of "staticConfig", how to configure the 'chirp' module and 'frame' module in "SensorConfig"? Should TX0 and TX2 be checked together and then set, or should TX0 and TX2 be configured separately?Whether TX0 and TX2 can be configured with different parameters ("Start freq var", "Freq Slope Vary", etc.)