Other Parts Discussed in Thread: LP-XDS110ET, LP-XDS110
你好
我们使用了AWRL1432雷达芯片设计了款产品,目前遇到关于下载和调试的问题。
在设计的时候TDI、TDO、TCK、TMS都有对应的接口,但是RS232的TX、RX并未连出。 因为串口并未连出,所以无法调试,我们计划使用JTAG烧录软件。
按照通常来讲JTAG可以支持烧录程序,但是在AWRL1432上没有明确的JTAG引脚。 请问XDS110还能支持进行烧录软件吗?如果可以,需要做哪些硬件上的什么设置?XDS110需要做那些调整呢?
感谢支持,期待您的回复。
Hello
We have used AWRL1432 radar chip to design a product, and now we have encountered problems in downloading and debugging.
In the design, TDI, TDO, TCK, TMS have corresponding interfaces, but the TX and RX of RS232 are not connected.
Because the serial port is not connected, it cannot be debugged. We plan to use JTAG burning software. Generally speaking, JTAG can support burning programs, but there is no explicit JTAG pin on AWRL1432.
Can XDS110 still support burning software? If so, what Settings on what hardware are required? What changes do you need to make to the XDS110?
Thank you for your support and look forward to your reply.