Part Number: PGA302
在使用PGA302芯片得时候,遇到以下现象:
此用于扭矩传感器上,在校准后,空载电压输出为2.5V,在产品上使用3个月后,空载输出电压变为了0V。重新校准可以恢复。但是为什么会出现一段时间后,输出变了得问题
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PGA302
在使用PGA302芯片得时候,遇到以下现象:
此用于扭矩传感器上,在校准后,空载电压输出为2.5V,在产品上使用3个月后,空载输出电压变为了0V。重新校准可以恢复。但是为什么会出现一段时间后,输出变了得问题
你好,
所有设备都会发生这种情况吗?或者只是一对?
设备中运行着一种补偿算法。校准系统时,该补偿算法的系数存储在EEPROM中。

一旦空载输出电压变为0V,系数是否符合您的预期?如中所示,它们是否与最初编程到设备的系数相同?
这是哪位客户?
一旦空载输出电压为0V,是否可以读取EEPROM系数?即使在装运时不知道系数,客户仍然可以知道EEPROM是否被擦除。例如,如果在空载输出电压为0V时所有系数都为零,即使设备在装运时已将系数编程到其中,这可能表明EEPROM受到了影响。