This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2733: LM2733YMFX/NOPB

Part Number: LM2733

TI官方标称LM2733YMFX/NOPB 工作电压范围2.7V-14V,我们实际测得正常LM2733最低工作电压1.4V左右,有较明显瞬时电流产生的LM2733最低工作电压1.8-2.0V左右;虽然目前LM2733的最低工作电压仍比标称的要好,但旧批次的LM2733可以在1.4V左右以上正常工作,而新批次的LM2733大部分(约80%)要在1.8V-2.0V以上才能正常工作。我们还是希望确认一下2025年至今,是否贵司对LM2733的规格或者生产工艺做过任何调整?或者,是否是因为产地不同,导致控制标准不同,最终导致产品各批次间存在这种差异?