This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3A27518E: 当通道内信号频率超过50MHZ时,部分器件的通信出现异常

Part Number: TS3A27518E


利用该器件连接SPI flash,用于不同主控制器的flash读取,但是当信号时钟速率超过50MHZ时,部分器件开始出现通信异常;另外当器件温度身高时,部分器件也会出现问题,读取的数据出错;感觉50Mhz是该款器件带宽的零界点;

工作电压为3.3V,请问这可能是什么引起的?

  • 您好,

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • 您好

    要通过多路复用器传递时钟信号(或任何方波),您应该始终选择带宽至少比时钟信号频率高5-7x的多路复用器。在这种情况下,TS3A27518E的带宽为240MHz,不到时钟频率50MHz的5倍。这可能就是你看到问题的原因。

    此外,该设备的额定温度为-40℃至85℃。如果您在这些温度之外使用它,我们无法提供性能数据。