项目需要测试神经元放电信号,信号放电幅值约几百uV。另外需要对神经元进行电刺激,电刺激电压幅值最大约10V。
问题:一共只有2个电极接入神经元,电刺激的2个电极和采集信号的2个电极想使用TMUX6236芯片进行模拟切换,请问方案是否可行?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
项目需要测试神经元放电信号,信号放电幅值约几百uV。另外需要对神经元进行电刺激,电刺激电压幅值最大约10V。
问题:一共只有2个电极接入神经元,电刺激的2个电极和采集信号的2个电极想使用TMUX6236芯片进行模拟切换,请问方案是否可行?
为了确保我理解正确,你是需要一个可以传递电压信号从微伏到10伏的多路复用器吗?这些是直流信号吗?如果不是,频率是多少?TMUX6236的带宽为40MHz。如果信号是直流的,那么TMUX6236在这里是可行的。
是一个一个可以传递电压信号从微伏到10伏的多路复用器,最小脉宽1us,可行吗?