Part Number: TLV61070A
你好,目前我使用TLV61070A设计一款升压电路,输入电压为2V~4.2V,输出电压为3.5V,当输入电压在3.4V以下时,电路无任何异常。当输入电压大于我的输出电压时,输出的两个22uF电容会发出啸叫,并且纹波有时高达150mV。请问在现有电路上需要怎么优化呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLV61070A
你好,目前我使用TLV61070A设计一款升压电路,输入电压为2V~4.2V,输出电压为3.5V,当输入电压在3.4V以下时,电路无任何异常。当输入电压大于我的输出电压时,输出的两个22uF电容会发出啸叫,并且纹波有时高达150mV。请问在现有电路上需要怎么优化呢?
您好,
您的问题可能是因为控制环路不稳定导致的啸叫以及纹波增大,您可以看看下面的内容能否对您的情况有所改善。
您可以看一下数据手册8.2.2.4 Loop Stability, Feedforward Capacitor Selection的建议,https://www.ti.com.cn/cn/lit/ds/symlink/tlv61070a.pdf
另外也请参考8.4.2 Layout Example
您也可以参考TLV61070A的开发板资源中的回路图以及layout,www.ti.com.cn/.../slvucc9.pdf
我使用的原理图 www.ti.com.cn/.../slvucc9.pdf 在此基础上取消了C2,C2改为22uF R2与R3合并为一个电阻600K R4 100K L1为6.8uH。我想知道这个芯片工作在直通模式时,是不是本身就是纹波比较大呢?