This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX131: AHD切换

Part Number: TMUX131

你好:TMUX131用于3路AHD信号切换是否合适。谢谢

  • 我对AHD信号并不十分熟悉,但从一些快速的研究来看,这些信号的频率范围在6MHz-45MHz之间。TMUX131的带宽为6.5GHz,因此就频率而言,使用该设备处理AHD信号是没有问题的。
    否则,AHD信号只需符合其他数据表规格,因此源极/漏极引脚上的最大电压为3.6V。