This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS5A22364-Q1: Latch-up current VS On-state switch peak current

Part Number: TS5A22364-Q1

 Latch-up performance meets 100 mA per AEC Q100-004. On-state switch peak current ±300mA. 

May I ask if in the LU test, the IO is capable of conducting a current of 300mA?

And in the LU test, do the other pins carry a current of 100mA?