This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3USB221 输入D+,D-pin是否可以互换?

Other Parts Discussed in Thread: TS3USB221

一般USB CONN和IC的D+,D- PIN与TS3USB221 的D+,D- PIN顺序相反,需要换层加VIA来routing,7,8pin D+,D-是否可以反接,即7 pin接D+输入信号,8 pin接D-输入信号,pin description没具体描述,帮忙确认,Thanks!

  • 您好,对于TS3USB221 来说,D—和D+ 电路是一样的,哪个做D+ , 哪个做D-都是可以的。
    如果按照您目前的接法,即只7,8 pinD+ 和D- 反接,而USB CONN 这边没有反接,那么当switch 导通之后,比如选择通道1, 那么7pin和1D1-连接,这样host的D+ 便接在了CONN的D-上, host 的D- 接在了CONN的D+上了。
    所以CONN和TS3USB221 端也可以反接,比如CONN的D+ 接1D-, 导通后,PIN2的1D-和PIN7的D-连接,而PIN7的D-接host的D+,这样host和CONN的极性是一致的。