Other Parts Discussed in Thread: TS5A23159
单刀单掷开关作为总线开关作用,当开关断开,下一节点脱离总线
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,485和CAN总线都是多大电压的? data rate为多少?
在选取开关器件时,要保证带宽和IO电压都满足,那么这款开关就是符合要求的.
电压是总线标准电压,485波特率115200,CAN速率 500K
您好,由于都是差分信号,所以您看下TS5A23159这款, 带宽100Mhz, 3.3V和5V都支持.