This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS5A23166: TS5A23166

Part Number: TS5A23166


你好:

     TS5A23166 芯片手册上说支持5V和3.3V。但是使用3.3V的时候,出现了开关常闭合的问题。

   1.   5V 系统    V+  =5V   Vin1 Vin2 控制电压是3.3V,这个没有问题,正常。

   2.  3.3V系统   V+  =3.3V   Vin1 Vin2 控制电压是3.3V,这个就有问题了,有时Vin1 给3.3V电压后,开关闭合,Vin1 给0V(GND)后,开关没有断开。

请问这是什么问题呢?

  • 您好,V+的范围为1.65V~5.5V,所以5V和3.3V都是没问题的。

    V+=3.3V时,控制电压Vih(min)=2V,所以给3.3V也没问题。另外,不用的通道不建议悬空, 建议上拉或接地。

      通过您的描述,应用应该是没问题的,换个通道试试呢?是否3.3V还是类似情况?

    或者建议您更换一片IC再试试是否还有类似问题?