This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G3157: SN74LVC1G3157和 TMUX1119 差異?

Part Number: SN74LVC1G3157
Other Parts Discussed in Thread: TMUX1119,

Dear :
SN74LVC1G3157和 TMUX1119 都是Analog Switch
在功能上有甚麼差異?
Thank
                                                        Roger Chang
  • 您好,功能上都是2:1 SPDT开关。TMUX1119属于精密开关器件,可以看下二者的数据手册,TMUX1119 的漏电流只有3pA。导通电阻Ron只有1.8ohm。并且内部集成Fail safe电路。 另外,逻辑控制端SEL 1.8V电平兼容,也就是说,即使5V供电,SEL可以使用1.8V逻辑,这也使得不少1.8V应用中的电平转换器件。