Part Number: TMUX6219
IC 只有D 接10V ,GND接地,VDD 就可以量到10V电压
请问是正确的吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMUX6219
IC 只有D 接10V ,GND接地,VDD 就可以量到10V电压
请问是正确的吗?
从最大电压额定值表格中可以看到,VS和VD的电压范围是VSS-0.5V 到 VDD+0.5V。
在VDD还没有供电时,VDD电压应该算是0V,VS或VD上如果输入电压,那就会大于VDD+0.5V,从而有永久性损害产品的可能。
总的来说,不管是VDD通电前还是通电过程中还是通电后,VS或VD的电压都不能超过VSS-0.5V ~ VDD+0.5V这个范围。