This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CB3T3245: 德州仪器TI规格书(SN74CB3T3245)中JESD 17如何理解?

Part Number: SN74CB3T3245


TI规格书(SN74CB3T3245)
Latch-Up Performance Exceeds 250 mA Per JESD 17如何理解?
请介绍下JESD 17。
谢谢!

  • 您好,

    JESD17是一个行业团队在1988年发布的第一个Latch-Up标准。

    Latch-Up是在电源引脚和接地之间创建低阻抗路径的一种情况。这种情况是由触发器(电流注入或过压)引起的,但一旦激活,即使触发器不再存在,低阻抗路径仍会保持。如果施加在设备上的电压和电流水平符合绝对最大额定值,则Latch-Up不存在风险。

    “Latch-Up Performance Exceeds 250 mA Per JESD 17 ” 意味着Latch-Up测试是在250mA峰值电流下进行的,并且设备通过测试,因此设备能够容忍大于250mA的Latch-Up事件。更多信息请查看下面文档:

    https://www.ti.com/lit/wp/scaa124/scaa124.pdf

  • 收到 谢谢解答。