This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HC4851-Q1: 注入电流保护

Part Number: SN74HC4851-Q1

 这里是不是意味着,只要我注入电流小于限制,我的输入电压是可以比VCC大的(VCC处添加稳压管)?如果是,那输入电压有上限吗还是只要电流满足就行那?

  • 您好,

    是的,输入的限值为“−0.5 V to VCC + 0.5 V”,意味着从输入到VCC和从输入到地之间有一个钳位二极管。在这种情况下,不允许输入电压高于VCC或低于0V,除非有一个串联电阻器将输入电流限制在小于IIK或IOK最大箝位电流额定值的范围内,但是这样二极管就会正偏导通,会向VCC反向供电。

    NOTE2提示,VIO电压最大5.5V。