Part Number: TS3V712E
请问TS3V712ERTGR和TS3V713ELRTGR这两颗器件有什么差异?看之前的回答感觉有点矛盾,没太看明白
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TS3V712E
请问TS3V712ERTGR和TS3V713ELRTGR这两颗器件有什么差异?看之前的回答感觉有点矛盾,没太看明白
TS3V712E: 3.3V 供电电压,输入5.5V tolerance,7通道的VGA开关器件。
TS3V712EL:L指的是level shifter, 和TS3V712E:的区别在于可以实现3.3V和5V之间的电平转换.
TS3V713EL和TS3V712EL的差异在于引脚排列的变化。
不知这样解释是否能明白,有问题再联系。


谢谢,这个有看到,但是看之前的回答有说到E版本是双向的,1:2或2:1都可以,EL是单向的,只能实现1:2,请问是这样的吗
您好,是的,您看下二者的内部架构,TS3V712E的为左侧图,它有两个控制端SEL1和SEL2分别控制A0~A4和A5~A6,如果VGA应用中A5和A6接HSYNC和VSYNC,可以看到A to B或者B to A都是可以的,双向的,但是对于712EL来说,这几个通道只有一个控制端SEL控制,而接Hysnc和Vsync可以看到是单向的,而SEL又控制了所有通道,所以这就决定了只能是1:2的这个方向。