Hi
帮确认一下,PTMUX4053PWR的电源电压最高能承受的工作电压
是正负双电源供电,是正负12V,还是正负14V,能不能在正负18V工作?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如工作电源为正负12V,是不是可以传导幅值为正负12V的信号,即可以正确导通负压信号?
是的;
如工作电源为正负14V,也是可以工作的,但有一定的风险?
是的,绝对最大额定电压是28V,若供电电压±14V存在波动超过28V就会有损坏设备的风险。超过推荐的工作条件VDD – VSS=24V,也不能保证其电气特性符合数据表中的参数。
那应该是没有申请权限,这属于非技术问题,如果您对此有疑问,请您按照以下方式联系客户支持部门,会有客服为您提供帮助。